DRV.NVVER
Description
Returns the version of Non Volatile Parameters stored. This version will change any time a non-backwards compatible change is made (i.e., the units of a keyword changes or scaling changes).
It is uncommon for this version to be incremented. If a parameter set is saved that is older than the firmware expects, Fault F1100 will be thrown and the user alerted that there was a failure loading parameters from internal flash memory.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
|
General Information
| Type | Read Only |
| Units | N/A |
| Range | N/A |
| Default Value | N/A |
| Data Type | String |
| Stored in Non-Volatile Memory | No |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
DRV.NVVER |
3000h |
0fh |
String(3) |
- |
- |
Read only |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
2012 |
1 |
2012 (0x7dc) |
DRV.NVVER |
String |
Read/Write |
No |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
DRV.NVVER |
2012 |
String |
Read/Write |
- |